LAPP

Digitalisation is reshaping public transport. Instead of simply transporting people from one stop to the next, modern vehicles now depend on a growing network of sensors, modules and control units. For operators, this means integrating complex digital systems into existing fleets while ensuring they remain robust and reliable in daily service.

Thoreb, a computer hardware specialist with a strong focus on intelligent transport systems, was tasked with upgrading a series of trams in Victoria. The project called for dependable connectivity that could withstand constant use in a demanding urban environment. As Ralf Otto, General Manager at Thoreb, explained: “All vehicles, from personal cars through to trains, buses and trams, have a series of sensors and modules, so to connect these together, gather data, and add functionality, there needs to be a ‘highway’ of reliable cables.”

Meeting these technical requirements was only part of the challenge, said Otto, which is why Thoreb partnered with LAPP Australia: “For a recent tram upgrade project, we chose LAPP Australia to provide cable assemblies, because not only did they provide the quality and reliability we were seeking, but they were willing to go above and beyond to meet tight deadlines and deliver to our customer’s precise requirements.”

LAPP Harnessing Solutions: certified, labelled, ready to Install

The cable assemblies, each rated with the appropriate rail certifications, were supplied by LAPP Australia’s new LAPP Harnessing Solutions division, which was set up to provide complete assemblies labelled, tested, and ready to go, to save time on automation projects.

“It was the personnel at LAPP that made this project possible, from quality control through to communications and final checks, they ticked all the boxes so that we could confidently deliver to our customer,” said Otto. “Additionally, as part of our proof of concept that we needed to deliver to the customer, all cables had to be clearly packed and labelled.”

“This is where LAPP Australia really stood out. Each assembly features a range of cables such as network cables, power cables, and earth cables, for four different classes of tram. Each component was labelled – at each end for cables – with what tram it belongs to, what type it is, and what its function is. They were then packed into kits that were clearly labelled as well,” he said. “This not only means that we can complete the installation accurately, but if we ever need to perform troubleshooting later on, we can isolate specific parts swiftly to reduce downtime.”

Connectivity powering smart functions

Thoreb’s solutions, enabled by LAPP Harnessing Solutions, support a wide range of functions that enhance the daily operation of trams: Passenger information screens inside the vehicles and external signage keep travellers informed about upcoming destinations or display important service messages. Sensors at the doors count how many people enter or leave, giving operators valuable data to adjust timetables and services to actual demand. Satellite links allow each tram to be tracked in real time, feeding information into passenger apps. In some cities, the system can even communicate with traffic lights to grant trams priority over cars, helping them stay on schedule.

Beyond these smart functions, the cabling also powers essential operations such as opening and closing doors, enabling stop buttons for passengers, and running the many electrical systems that keep the tram safe and comfortable.

“With so many cables in a small space, electrical emissions could create too much noise pollution and reduce the performance of the system, or the comfort of passengers, but LAPP’s cables have electromagnetic interference shielding properties to protect against this issue,” said Otto.

Reliable partnership across state lines

Meeting the demands of this tram upgrade required precise coordination. Thoreb’s head office in New South Wales worked hand in hand with project teams in Victoria, while LAPP Australia supported the process at every stage. With tight deadlines and work spread across state lines, clear communication proved essential.

Ralf Otto emphasized how much this mattered to the outcome: “LAPP kept us well informed throughout the process. What we particularly liked was that they informed us if there were any delays. Some companies don’t like to deliver negative news, but we are aware that sometimes there are delays outside of their control, and learning about it as early as possible helps us plan accordingly.”

For him, the partnership went beyond technical delivery: “Our experience with the LAPP Australia team was that they were reliable, trustworthy, and respectful. We hope to be able to work with them again on future projects.”