Most of the time, the issues don’t come from one big mistake. They come from small decisions that seem reasonable on their own, but start to create friction once everything is put together.
These patterns show up again and again across projects.
1. Testing is treated as a final step
At first, everything looks correct. The harness meets specifications, connections are in place, and basic checks pass. The problems appear later.
A connection behaves differently under load, a signal isn’t as stable as expected, or something that worked in isolation starts failing within the system. By that point, fixing it is no longer simple.
2. Components come from everywhere
One supplier for cables, another for connectors, another for assembly. It works — until something doesn’t.
When issues appear, it’s no longer clear where responsibility sits. Time is spent aligning between parties instead of solving the actual problem.
3. Integration is left to the last moment
On paper, everything fits. Installation takes longer. Components don’t align as expected.
Small mismatches turn into adjustments — and adjustments start to add up. What should have been straightforward becomes something that needs to be figured out on site.
4. One missing part stops everything
A system is nearly complete — and then it waits.
Not because of complexity, but because a single component is delayed or unavailable. At that point, even a small dependency becomes a blocker.
5. “We’ll do it in-house” seems efficient
At the beginning, it often is. Then the volume increases, variants grow, and changes start coming in.
What used to be manageable starts taking time — from engineering, from production, and from people who were meant to focus elsewhere. And slowly, it becomes a bottleneck.
Most harnessing issues don’t come from dramatic failures. They come from small things that only become visible once everything comes together — when time is limited, and changes are harder to absorb.
That’s where cost is really created.
LAPP Harnessing Solutions
LAPP Harnessing Solutions supports these situations across the full process — from design and sourcing to assembly and testing — so that harnessing doesn’t become the part that slows everything else down.