This was precisely the situation faced by a manufacturer of such aircraft tow tractors, whose vehicles are becoming increasingly complex in technical terms and contain more and more electrical components. “The customer was looking for a partner who would take on more than just the supply of components. Our aim from the outset was therefore to provide as much added value as possible and to deliver ready-to-install solutions,” explains Anna Schüller, Business Development Harnessing at LAPP. In addition to high product quality, the customer’s key requirements were, above all, delivery reliability, technical support and the ability to relieve the strain on their own production facilities. The collaboration with LAPP, one of the leading providers of integrated solutions in the field of cable and connection technology, began in early 2025 through LAPP’s field sales team and quickly developed into a joint development project. Until then, the customer had been manufacturing some of its cable assemblies and complex box-build solutions in-house, thereby tying up resources that were actually needed elsewhere. “As air traffic had picked up again, demand for the customer’s aircraft tugs also rose,” explains Anna Schüller. However, the increase in production was becoming an ever-greater challenge for the customer. The manufacturer was therefore looking for a partner who could take on complete electrical assemblies and clarify technical issues directly with the relevant specialists.
High-voltage cables for the drive system
The high-voltage cables required play a key role in electric aircraft tugs. They transmit energy from the battery system to the drive and must operate reliably under a wide variety of environmental conditions – in other words, they must meet requirements that a standard cable does not always fulfil. The technical solution was found within the LAPP Group: the Italian LAPP team already had a high-voltage silicone cable, the ÖLFLEX® HV EV, which was suitable for the customer’s demanding environment. “The great thing about this project was that we were able to draw very quickly on the expertise and solutions within the LAPP Group to find the best solution for the customer’s specific application,” said Schüller. There were also good reasons for the choice of material: aircraft tugs operate outdoors all year round and must withstand both low temperatures in winter and summer heat. The cable’s silicone sheath remains flexible even in cold conditions, is temperature-resistant and, compared to sheaths made of PUR or PVC, makes installation easier in challenging situations. Even the relatively large cable cross-section of 95 mm²required for the solution posed no problem for LAPP.
Bespoke high-voltage assemblies
The next step was to manufacture ready-to-install high-voltage assemblies from the cables. Reproducible manufacturing processes and reliable quality assurance were particularly important here. “With high-voltage applications, it is not enough simply to carry out individual work steps correctly. It is crucial that every process functions reliably and that every assembly is precisely tested. That is why, together with our colleagues, we coordinated the manufacturing and testing procedures in detail,” explains Schüller. The result was a solution precisely tailored to the requirements of the customer’s new generation of vehicles.
In parallel with the high-voltage assemblies, LAPP also took on the manufacture of complete box-build solutions for the customer, thereby further easing the burden on their production.
From component supplier to system partner
LAPP now manufactures several variant assemblies for the manufacturer, comprising a total of more than 290 different components. Before delivery, more than 600 test points are checked for each assembly. “We were able to support the customer in two areas at once,” says Anna Schüller. “On the one hand, with high-voltage assemblies, and on the other, with electrical sub-assemblies. We set up a new test facility specifically for this purpose. This ensures the customer receives fully tested solutions that are ready for immediate use.”
What began in early 2025 as a joint search for a suitable high-voltage solution has since developed into a comprehensive partnership that is set to be expanded even further. “For our customers, it is no longer just about finding the right cable, but about the entire connection solution. This is precisely where we can pool our strengths and provide our customers with long-term relief,” summarises Schüller. Both companies intend to continue working together in the future. “We have found that both companies are structured in a similar way and are alike in many respects. And thanks to this strong partnership, we can offer customers one-to-one support and constant availability for all challenges.”